FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding the Mark detection function
FAQ
Regarding the Mark detection function
Motion module: Is the Mark detection function used in the FX5 40/80SSC-G compatible with the built-in motion function of the MX-F Model?
Answer
The Mark detection function of the FX5-40/80SSC-G is supported by the Touch probe function of the MX-F Model.
- Product Name
- MX-F Model
- Series
- MELSEC MX Controller