FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Port No. in Connected Ethernet Controller Setting when connecting the MELSEC iQ-F series via Ethernet
FAQ
Port No. in Connected Ethernet Controller Setting when connecting the MELSEC iQ-F series via Ethernet
When connecting the MELSEC iQ-F series (FX5U, FX5UC, FX5UJ, or FX5S) via Ethernet, what should be set for Port No. in Connected Ethernet Controller Setting?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
When connecting the MELSEC iQ-F series (FX5U, FX5UC, FX5UJ, or FX5S) via Ethernet, set Port No. in Connected Ethernet Controller Setting as shown in Table 2.
Select "FX5CPU" for the Unit Type field in Connected Ethernet Controller Setting.
◆ For GT Designer3 (GOT2000) Version 1
Figure 1: Port No. in Connected Ethernet Controller Setting

Table 2: Port No. to set for the controller in Connected Ethernet Controller Setting

○: Can be set, -: Cannot be set
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT2000 Series, SoftGOT2000, GOT3000 Series, SoftGOT3000