FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > Limiting numerical display, numerical input, text display, and text input using level authentication (password authentication)
FAQ
Limiting numerical display, numerical input, text display, and text input using level authentication (password authentication)
How do I restrict numerical display, numerical input, text display, and text input using level authentication?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
The following shows how to limit numerical display, numerical input, text display, and text input using level authentication.
Configure the settings in the screen design software.
(Example) Limiting numerical input with a security level.
The security level settings are as follows:
• Display: 0 (All users) / Input: 10 or more
• Security level device: GD200
◆ GT Designer3 (GOT3000) Version 1
1. Set the security mode to [Mode 1]
• In [Type Setting], select [Security Setting] → [Mode 1 (GOT2000 Series Compatible].
2. Set the screen security level (level authentication) if it is not already set
• Select [Common] → [GOT Environmental Setting] → [Security] then select the [Screen Security] tab and select [Level] for the authentication method.
3. Open the [Numerical Input] setting dialog, select the [Extended] tab and set [Security Level].
• [Display]: 0 / [Input]: 10
4. Place a special function switch on the base screen for logging in.
Open the [Special Function Switch] setting dialog, and set [Switch Action] to [Password (Security level)].
5. Place a word switch on the base screen for logging out.
Open the [Word Switch] setting dialog and configure each setting.
• [Device]: GD200 / [Constant]: Select this item and set it to "0".
◆ Operation on the GOT
1. Touch the special function switch for logging in and enter the password that corresponds to the security level on the password screen.
2. To log out, touch the word switch for logging out.
For information on setting level authentication, refer to the screen design software manual.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (numerical display/text display), GOT function (numerical input/text input), GOT function (level authentication)
- Series
- GOT3000 Series, GOT Screen Design Software, SoftGOT3000