Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 45283
  • Release Date : 2025/10/22 17:11
  • Print

Reasons for slow screen switching

Answer

Possible causes of slow screen switching are as follows:

• The incorrect communication driver is selected.
• When connected via Ethernet, a device with a duplicate IP address or station number is connected.
• The baud rate is incorrect for serial connection.
• When connected via Ethernet, a communication timeout has occurred on a channel.
• The execution cycle of background processes (scripts, logging, etc.) is short.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series, SoftGOT2000, GOT3000 Series, SoftGOT3000

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries