FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Setting the PLC station number when connecting the GOT to the PLC via Ethernet
FAQ
Setting the PLC station number when connecting the GOT to the PLC via Ethernet
How do I set the PLC station number when connecting the GOT to the PLC via Ethernet?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
The following shows how to set the PLC station number when connecting the GOT to the PLC via Ethernet.
Configure the settings in the screen design software.
◆ For GT Designer3 (GOT2000) Version 1
[Common] → [Controller Setting] → [Connected Ethernet Controller Setting]
Ensure that [GOT Station] and [Station] are not duplicated in Connected Ethernet Controller Setting.
Figure 1

- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT3000 Series, GOT2000 Series, SoftGOT3000, SoftGOT2000