• No : 21250
  • Release Date : 2018/08/22 16:26
  • Print

Proportional band of multiple inverters

I want to perform proportional band of three inverters by changing the speed of one inverter. How should I input the inverter analog output to the second inverter?
Category : 

Answer

By importing the operation frequency from the AM terminal (analog output) of the first inverter to the FR-FH (ratio setter), the operation command which is proportional to other three inverters can be sent.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700