- No : 21251
- Release Date : 2018/08/22 16:26
-
Print
Frequency command
I want to use the frequency 0.49 Hz for operation but FWD blinks and operation does not start. (I can use 0.9 Hz for operation.) How should I configure the setting?
- Category :
-
Answer
Since the initial value of Pr.13 (Starting frequency) is 0.5 Hz, the operation does not start unless 0.5 Hz or higher frequency is set. When 0.49 Hz is set in Pr.13, operation starts at 0.49 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700