• No : 21251
  • Release Date : 2018/08/22 16:26
  • Print

Frequency command

I want to use the frequency 0.49 Hz for operation but FWD blinks and operation does not start. (I can use 0.9 Hz for operation.) How should I configure the setting?
Category : 

Answer

Since the initial value of Pr.13 (Starting frequency) is 0.5 Hz, the operation does not start unless 0.5 Hz or higher frequency is set. When 0.49 Hz is set in Pr.13, operation starts at 0.49 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700