- No : 21270
- Release Date : 2018/08/22 16:26
-
Print
Parameter setting
Can I input the single-phase 200 V only when setting the parameter of the inverter?
- Category :
-
Answer
Yes. The single-phase 200 V can be input.
If the single-phase input is performed when Pr.872 (Input phase loss protection) is set to "1", the input phase loss (E.ILF) error may occur, but the parameters can be set.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700