• No : 21270
  • Release Date : 2018/08/22 16:26
  • Print

Parameter setting

Answer

Yes. The single-phase 200 V can be input.
If the single-phase input is performed when Pr.872 (Input phase loss protection) is set to "1", the input phase loss (E.ILF) error may occur, but the parameters can be set.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700