- No : 21280
- Release Date : 2018/08/22 16:26
-
Print
Rated frequency setting
When the spindle motor with 200 Hz rated frequency is used, "OL" (overload) is displayed at 4 to 5 Hz and the speed does not increase.
How should I configure the setting?
- Category :
-
Answer
Check that Pr.3 (Base frequency) is set to "200 Hz".
Adjust Pr.0 (Torque boost) as necessary.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700