- No : 21284
- Release Date : 2018/08/22 16:26
-
Print
Frequency
When the output frequency is increased from 60 Hz to 80 Hz, how much does the motor torque decreases?
- Category :
-
Answer
When the torque is supposed as 100% at 60 Hz, the torque becomes 75 % at 80 Hz.
(Under V/F control, the torque decreases when the frequency exceeds 60 Hz because the voltage over a certain limit cannot be output.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700