• No : 21284
  • Release Date : 2018/08/22 16:26
  • Print

Frequency

When the output frequency is increased from 60 Hz to 80 Hz, how much does the motor torque decreases?
Category : 

Answer

When the torque is supposed as 100% at 60 Hz, the torque becomes 75 % at 80 Hz.
(Under V/F control, the torque decreases when the frequency exceeds 60 Hz because the voltage over a certain limit cannot be output.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700