- No : 21295
- Release Date : 2018/08/22 16:26
-
Print
Error "E.UVT" (undervoltage protection)
The inverter has been operating normally, but an error "E.UVT" (undervoltage protection) has displayed and tripped.
What are the possible causes?
- Category :
-
Answer
The possible causes of the error UVT are as follows.- Low power supply voltage
- Insufficient power supply capacity
- Damage or failure Check the power supply voltage and voltage of the terminals P and N of the inverter.
If there is no problem, the parts may be damaged or broken.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700