- No : 21305
- Release Date : 2018/08/22 16:26
- 
          
              Print
          
        
 
Number of stations that can be set in FR Configurator
    
      I want to connect FR-Configurator (FR-SW3-SETUP-WJ) setup software using the USB. 
It seems like station numbers 0 to 31 can be set. Can I arrange them individually?  
    
  
    - Category : 
- 
      
    
 
    Answer
  
    The station numbers that can be set differ depending on the version of FR-Configurator (FR-SW3-SETUP-WJ) setup software. 
For Ver.2.00 or later, station numbers 0 to 31 can be individually set. 
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700