- No : 21312
 
      - Release Date : 2018/08/22 16:26
 
        - 
          
              Print
          
        
 
  
 
Connection cable of FR-Configurator
    
      I want to communicate with FR-Configurator (FR-SW3-SETUP-WJ) using the USB connector. 
Is the Mini-B indicates the standardized Mini-B connector?   
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    It is the standardized Mini-B connector.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700