• No : 21312
  • Release Date : 2018/08/22 16:26
  • Print

Connection cable of FR-Configurator

I want to communicate with FR-Configurator (FR-SW3-SETUP-WJ) using the USB connector.
Is the Mini-B indicates the standardized Mini-B connector?
Category : 

Answer

It is the standardized Mini-B connector.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700