- No : 21326
- Release Date : 2018/08/22 16:27
-
Print
Capacity selection
How can I select the inverter capacity when using a motor?
- Category :
-
Answer
Select the inverter capacity so that the rated output current of inverter ? rated motor current × 1.1.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700