• No : 21329
  • Release Date : 2018/08/22 16:27
  • Print

Brake resistor

Is only one resistor used for the high-duty brake resistor FR-ABR-15K (inverter option)?
Category : 

Answer

Use two resistors for the high-duty brake resistor FR-ABR-15K. (Connect two resistors of 18 ? in parallel.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700