- No : 21329
- Release Date : 2018/08/22 16:27
-
Print
Brake resistor
Is only one resistor used for the high-duty brake resistor FR-ABR-15K (inverter option)?
- Category :
-
Answer
Use two resistors for the high-duty brake resistor FR-ABR-15K. (Connect two resistors of 18 ? in parallel.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700