- No : 21330
- Release Date : 2018/08/22 16:27
-
Print
Brake resistor
I do not have the high-duty brake resistor FR-ABR-1.5K (inverter option). Which brake resistor should I use for the inverter with capacity of 1.5K?
- Category :
-
Answer
Use high-duty brake resistor FR-ABR-2.2K. (Shared with the 1.5K inverter.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700