- No : 21330
- Release Date : 2018/08/22 16:27
- 
          
              Print
          
        
 
Brake resistor
    
      I do not have the high-duty brake resistor FR-ABR-1.5K (inverter option). Which brake resistor should I use for the inverter with capacity of 1.5K?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    Use high-duty brake resistor FR-ABR-2.2K. (Shared with the 1.5K inverter.)
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700