• No : 21331
  • Release Date : 2018/08/22 16:27
  • Print

Brake resistor

Is the brake resistor MYS120W40 (inverter option) shared when the inverter capacity of 2.2K and 3.7K are used?
Category : 

Answer

It will be the shared type.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700