- No : 21331
- Release Date : 2018/08/22 16:27
-
Print
Brake resistor
Is the brake resistor MYS120W40 (inverter option) shared when the inverter capacity of 2.2K and 3.7K are used?
- Category :
-
Answer
It will be the shared type.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700