• No : 21336
  • Release Date : 2018/08/22 16:27
  • Print

Parameter

Answer

Press the "MODE" key on the operation panel several times to display "P.0" and parameter setting screen.
Then turn the setting dial to display "C..." screen and press the "SET" key.
The display changes to "C---". Turn the setting dial again to the parameter C□ to be calibrated, then press the "SET" key.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700