- No : 21336
 
      - Release Date : 2018/08/22 16:27
 
        - 
          
              Print
          
        
 
  
 
Parameter
    
      How can I read the calibration parameter Pr.C of the inverter parameter?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Press the "MODE" key on the operation panel several times to display "P.0" and parameter setting screen. 
Then turn the setting dial to display "C..." screen and press the "SET" key. 
The display changes to "C---". Turn the setting dial again to the parameter C□ to be calibrated, then press the "SET" key.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700