- No : 21360
- Release Date : 2018/08/22 16:27
-
Print
MRS setting
1. What is the difference between MRS and Pr.250 = "0"?
2. Do I have to set both of them?
- Category :
-
Answer
1. For MRS, coasting starts when the MRS contact turns ON. For Pr.250 = "0",IM is coasting immediately when the start signal is turned OFF.
2. No. Set either one.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700