• No : 21360
  • Release Date : 2018/08/22 16:27
  • Print

MRS setting

1. What is the difference between MRS and Pr.250 = "0"?  

2. Do I have to set both of them?
Category : 

Answer

1. For MRS, coasting starts when the MRS contact turns ON. For Pr.250 = "0",IM is coasting immediately when the start signal is turned OFF.  

2. No. Set either one.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700