• No : 21674
  • Release Date : 2018/08/22 16:28
  • Print

Network operation

I am planning to operate the inverter over the network, and I want to input the start signal (STF) from the network and use an external analog signal 4 to 20 mA DC to set the frequency.
How should I set Pr.338 (Communication operation command source) and Pr.339 (Communication speed command source)?
Category : 

Answer

Set Pr.338 to "0" (NET) and Pr.339 to "1" or "2".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700