• No : 21746
  • Release Date : 2018/08/22 16:29
  • Print

Package

Answer

It is the fixing screw for the inverter cooling fan cover.

The size and number of screws depend on the model and capacity.

(When exporting the product to the EU, this screw fixes the fan cover so that it would not come off during transport.
It is not necessary when the product is used in Japan.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700