- No : 21920
- Release Date : 2018/08/22 16:30
- 
          
              Print
          
        
 
Using external potentiometer and multi-speed operation together
    
      Can I use an external potentiometer and multi-speed operation together?
If I use them together, which frequency setting is enabled?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    You can use an external potentiometer and multi-speed operation together.
When an external potentiometer signal input and multi-speed setting occur simultaneously, multi-speed setting is prioritized.
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700