• No : 21920
  • Release Date : 2018/08/22 16:30
  • Print

Using external potentiometer and multi-speed operation together

Can I use an external potentiometer and multi-speed operation together?
If I use them together, which frequency setting is enabled?
Category : 

Answer

You can use an external potentiometer and multi-speed operation together.
When an external potentiometer signal input and multi-speed setting occur simultaneously, multi-speed setting is prioritized.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700