- No : 23614
 
      - Release Date : 2018/09/14 15:09
 
        - 
          
              Print
          
        
 
  
 
Error 1205
    
      What is error 1205?
What should I do when it occurs?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Error 1205 (SSCNET communication error) occurs when erroneous data is received from servo amplifier.
[When the servo parameter "[PA14] Rotation direction selection/travel direction selection" is changed]
Execute the home position return again.
[When the servo parameter "[PA14] Rotation direction selection/travel direction selection"  is not changed]
• Check if the SSCNETIII cable and the encoder cable are connected correctly.
• Take measures against noise.
  
    
      
        - Product Name
 
          - Simple Motion module/
Positioning module 
      
      
        - Series
 
          - MELSEC-Q
MELSEC-L