FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-R2R
FAQ
FR-A800-R2R
What is the initial winding diameter value when the initial winding diameter calculation is not performed?
- Category :
Answer
When the value is written to Pr.646 (Stored winding diameter), the stored value is used. When the value is not written, the minimum or maximum winding diameter value is used. Which one to be used depends on whether the operation is winding or unwinding. (minimum value at the winding/maximum value at the unwinding)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-R2R