FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-R2R
FAQ
FR-A800-R2R
How is the initial roll calculated?
- Category :
Answer
The calculation is performed by two modes. One method calculates the current winding diameter automatically by moving the dancer roll from lower limit position to the target position at start. The other method calculates the current winding diameter from the line speed and actual rotation speed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800 Plus