FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > CC-Link
FAQ
CC-Link
When the MRS (output shutoff) signal is input during operation, the output frequency monitor value becomes "0". However, when the inverter stops by such as external thermal abnormal occurrence, an error occurred is held and the output frequency monitor value does not become "0". Why is that?
- Category :
Answer
It is because the CC-Link monitor is designed to hold the value at an error occurrence.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option