FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Anti-sway control
FAQ
Anti-sway control
It is describes that when Pr.1074 is set to "9999", the anti-sway control is performed using a swinging frequency estimated by the inverter according to the settings of Pr.1077 to Pr.1079. When the load weight is 1 to 5 kg, what value should I set?
- Category :
Answer
Set 3 kg (intermediate value) for the load weight 1 to 5 kg.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800