FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-R2R
FAQ
FR-A800-R2R
How the system can be simplified with the Roll to Roll dedicated inverter?
- Category :
Answer
When the winding ratio is large, the control according to the winding diameter is required. The upper controller has measured the winding diameter and created the command for the inverter. With the Roll to Roll dedicated machine, the control that have been performed in combination with the controller can be achieved by the inverter alone. Construction of small and medium size systems has become much more simple.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800