FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800
FAQ
FR-A800
Though the control circuit temperature can be monitored with Pr.52=98, is any alarm generated when the control circuit temperature rises?
- Category :
Answer
No alarm occurs due to the abnormal temperature. In the main circuit, alarms such as heatsink overheat will be occurred.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800