FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Overseas inverter models
FAQ
Overseas inverter models
What is the naming convention for the overseas inverter models?
Are there any rules for kw?
Are there any rules for kw?
- Category :
Answer
"□□□□□" in the model name of the FR-A700 series and FR-F700 series with the multiple ratings is as follows.
"□□□□□" in the model name of the FR-A700 series and FR-F700 series with the multiple ratings is as follows.
FR-[A/F]7[2/4]0-□□□□□-NA/EC
- For the FR-A700 series in Europe (EC): SLD rated output current value
- For the FR-A700 series in North America (NA): ND rated output current value
- For the FR-F700 series in Europe (EC): SLD rated output current value
- For the FR-F700 series in North America (NA): SLD rated output current value
For example, when the rated output current value is 4.6 A, "□□□□□" is "00046", and when the rated output current value is 475 A, it is "04750".
"□□□□□" in the model name of the FR-A700 series and FR-F700 series with the multiple ratings is as follows.
FR-[A/F]7[2/4]0-□□□□□-NA/EC
- For the FR-A700 series in Europe (EC): SLD rated output current value
- For the FR-A700 series in North America (NA): ND rated output current value
- For the FR-F700 series in Europe (EC): SLD rated output current value
- For the FR-F700 series in North America (NA): SLD rated output current value
For example, when the rated output current value is 4.6 A, "□□□□□" is "00046", and when the rated output current value is 475 A, it is "04750".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700