FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > MM-FR-A800
FAQ
MM-FR-A800
What is the minimum frequency of the point table positioning with the MM-CF?
- Category :
Answer
If the command is 0.01 Hz or higher, the positioning control is performed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800