FAQ


FAQAbout Products
 
 - FAQ > Drive Products > Inverters-FREQROL > Engineering Software > FR Configurator2
FAQ
FR Configurator2
      When editing the USB memory parameter copy file, the CP1 file is specified and edited. Can I generate a new CP1 file and transfer it to the inverter without using the existing CP1 file?
    
  - Category :
Answer
    Only the parameter setting values (USB memory parameter copy file: CP1 file) read from the inverter to USB memory can be edited. Customers cannot generate a CP1 file.
  
    - Product Name
- Inverter, magnet motor drive
- Product Category
- Engineering software
- Series
- Option