FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > Simple magnetic flux vector control
FAQ
Simple magnetic flux vector control
When Pr.80 and Pr.81 are set, the simple magnetic flux vector control is used in the FR-F700P; however, the advanced magnetic flux vector control is used in the FR-F800 instead. Is the simple magnetic flux vector control not available for the FR-F800?
- Category :
Answer
The simple magnetic flux vector control is unavailable for the FR-F800. The advanced magnetic flux vector control is higher-level function of the simple magnetic flux vector control. Thus, the advanced magnetic flux vector control is used in the FR-F800.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F800