FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > PM motor control
FAQ
PM motor control
For the FR-F700P, the control method is IPM motor drive and for the FR-F800, it is PM motor drive. Are there any differences?
- Category :
Answer
For the FR-F700P, only dedicated IPM motor (MM-EFS, MM-THE4) can be driven. For the FR-F800, the name is different because PM motors manufactured by other companies can be driven by performing offline auto tuning.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F800