FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A800
FAQ
FR-A800
Are the number of output terminals and terminal function selection the same as those of the A700 series?
(For A700: RUN, SU, IPF, OL, FU, ABC)
(For A700: RUN, SU, IPF, OL, FU, ABC)
- Category :
Answer
Number of terminals: There are the same output terminals as A700 and the following terminals (2 points) are added. Safety: SO, SOC * The terminals SO and SOC are dedicated to the safety. The function cannot be changed as other terminals.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800