FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-HC2
FAQ
FR-HC2
What is the measurement method and accuracy of the input current monitor?
- Category :
Answer
Three phases are measured with the CT. The accuracy is ±10 % which is same as the inverter output current.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Option