FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-HC2
FAQ
FR-HC2
The MC1 in the outside box (FR-HCB2) is chattering. What is the possible cause?
- Category :
Answer
The power of MC1 is supplied from the terminals across R2 and S2 of the outside box. Either phase of R2 or S2 may be lost.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Option