FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FR Configurator SW3 (CC-Link Seamless)
FAQ
FR Configurator SW3 (CC-Link Seamless)
Why is "Error: 0X80010016" displayed when Pr.77 (Parameter write selection) and Pr.79 (Operation mode selection) are written via CC-Link communication.
- Category :
Answer
Pr.77 and 79 cannot be changed via CC-Link communication.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Others