FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-B3
FAQ
FR-B3
The carrier frequency can be set in Pr.72 (PWM frequency selection) for the FR-B, but it cannot be set for the FR-B3. What is the carrier frequency (kHz) set for the FR-B3?
- Category :
Answer
The carrier frequency for the FR-B3 is 2 kHz. For the low noise type FR-B3-N, it is 14.5 kHz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Option