FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Reverse operation
FAQ
Reverse operation
I want to perform a test run in reverse operation with RUN.
- Category :
Answer
Reverse operation is enabled by changing the setting of Pr.40.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ